Applications - Memory Occupancy#

Below is the memory occupancy of the default examples with 3.3.1 release (M4 - Application processor). The following memory occupancy may vary from release to release for a common flash device (8 MB).

Example Name

Features

Flash

RAM

wifi_station_ble_provisioning_aws

Wi-Fi, Cloud, SSL, Certificates

66 KB

129 KB

wifi_http_otaf

Wi-Fi, HTTP, TCP/IP

40 KB

96 KB

wifi_powersave_standby_associated_soc

Wi-Fi, Power-save

44 KB

102 KB

wifi_station_ble_throughput_app

Wi-Fi, BLE, TCP/IP

49 KB

100 KB

Note: The leftover RAM will be allotted to ‘.heap’ variable.