QEI interrupt acknowledge structure.
This structure contains flags for acknowledging different interrupt levels for the QEI.
Public Attributes#
uint32_t
Position count reset interrupt level.
uint32_t
Index count match interrupt level.
uint32_t
Position counter error interrupt level.
uint32_t
Velocity less than interrupt level.
uint32_t
Position count match interrupt level.
uint32_t
Velocity computation over interrupt level.
Public Attribute Documentation#
qei_position_cnt_reset_intr_lev#
uint32_t sl_qei_intr_ack_t::qei_position_cnt_reset_intr_lev
Position count reset interrupt level.
qei_index_cnt_match_intr_lev#
uint32_t sl_qei_intr_ack_t::qei_index_cnt_match_intr_lev
Index count match interrupt level.
qei_position_cntr_err_intr_lev#
uint32_t sl_qei_intr_ack_t::qei_position_cntr_err_intr_lev
Position counter error interrupt level.
qei_velocity_less_than_intr_lev#
uint32_t sl_qei_intr_ack_t::qei_velocity_less_than_intr_lev
Velocity less than interrupt level.
qei_position_cnt_match_intr_lev#
uint32_t sl_qei_intr_ack_t::qei_position_cnt_match_intr_lev
Position count match interrupt level.
qei_velocity_computation_over_intr_lev#
uint32_t sl_qei_intr_ack_t::qei_velocity_computation_over_intr_lev
Velocity computation over interrupt level.