QEI interrupt unmask structure.
This structure defines unmasking options for various QEI interrupts, allowing them to be enabled.
Public Attributes#
uint32_t
Unmask for position count reset interrupt.
uint32_t
Unmask for index count match interrupt.
uint32_t
Unmask for velocity less than interrupt.
uint32_t
Unmask for position counter error interrupt.
uint32_t
Unmask for position count match interrupt.
uint32_t
Unmask for velocity computation over interrupt.
Public Attribute Documentation#
qei_position_cnt_reset_intr_unmask#
uint32_t sl_qei_intr_unmask_t::qei_position_cnt_reset_intr_unmask
Unmask for position count reset interrupt.
qei_index_cnt_match_intr_unmask#
uint32_t sl_qei_intr_unmask_t::qei_index_cnt_match_intr_unmask
Unmask for index count match interrupt.
qei_velocity_less_than_intr_unmask#
uint32_t sl_qei_intr_unmask_t::qei_velocity_less_than_intr_unmask
Unmask for velocity less than interrupt.
qei_position_cntr_err_intr_unmask#
uint32_t sl_qei_intr_unmask_t::qei_position_cntr_err_intr_unmask
Unmask for position counter error interrupt.
qei_position_cnt_match_intr_unmask#
uint32_t sl_qei_intr_unmask_t::qei_position_cnt_match_intr_unmask
Unmask for position count match interrupt.
qei_velocity_computation_over_intr_unmask#
uint32_t sl_qei_intr_unmask_t::qei_velocity_computation_over_intr_unmask
Unmask for velocity computation over interrupt.