LFN network parameters.
Public Attributes#
uint16_t
Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).
uint8_t
Duration for which an LFN waits for a registration confirmation (minutes).
uint8_t
Reserved, set to zero.
Public Attribute Documentation#
lfn_registration_lifetime_m#
uint16_t sl_wisun_lfn_params_network_t::lfn_registration_lifetime_m
Address registration lifetime (IPv6 lease duration) the LFN requires to the Border Router (minutes).
Specification range [1440, 5040]
Definition at line
87
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
lfn_na_wait_duration_m#
uint8_t sl_wisun_lfn_params_network_t::lfn_na_wait_duration_m
Duration for which an LFN waits for a registration confirmation (minutes).
Specification range [30, 120]
Definition at line
90
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
reserved#
uint8_t sl_wisun_lfn_params_network_t::reserved
Reserved, set to zero.
Definition at line
92
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h