LFN parameter set.
Public Attributes#
uint32_t
Version of this API.
LFN connection parameters.
LFN data layer parameters.
LFN network parameters.
LFN power parameters.
Public Attribute Documentation#
version#
uint32_t sl_wisun_lfn_params_t::version
Version of this API.
This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.
Definition at line
123
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
connection#
sl_wisun_lfn_params_connection_t sl_wisun_lfn_params_t::connection
LFN connection parameters.
Definition at line
125
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
data_layer#
sl_wisun_lfn_params_data_layer_t sl_wisun_lfn_params_t::data_layer
LFN data layer parameters.
Definition at line
127
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
network#
sl_wisun_lfn_params_network_t sl_wisun_lfn_params_t::network
LFN network parameters.
Definition at line
129
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h
power#
sl_wisun_lfn_params_power_t sl_wisun_lfn_params_t::power
LFN power parameters.
Definition at line
131
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h