Custom QPSK PHY configuration.

Public Attributes#

uint32_t

Ch0 center frequency in kHz.

uint16_t

Channel spacing in kHz.

uint16_t

Number of channels.

uint8_t

PHY mode ID.

uint8_t
uint8_t

OQPSK preamble length in bits.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

ch0_frequency_khz#

uint32_t sl_wisun_phy_config_custom_oqpsk_t::ch0_frequency_khz

Ch0 center frequency in kHz.


Definition at line 589 of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

channel_spacing_khz#

uint16_t sl_wisun_phy_config_custom_oqpsk_t::channel_spacing_khz

Channel spacing in kHz.


Definition at line 591 of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

number_of_channels#

uint16_t sl_wisun_phy_config_custom_oqpsk_t::number_of_channels

Number of channels.


Definition at line 593 of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

phy_mode_id#

uint8_t sl_wisun_phy_config_custom_oqpsk_t::phy_mode_id

PHY mode ID.


Definition at line 595 of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

crc_type#

uint8_t sl_wisun_phy_config_custom_oqpsk_t::crc_type

OFDM CRC type (sl_wisun_crc_type_t)


Definition at line 597 of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

preamble_length#

uint8_t sl_wisun_phy_config_custom_oqpsk_t::preamble_length

OQPSK preamble length in bits.


Definition at line 599 of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h

reserved#

uint8_t sl_wisun_phy_config_custom_oqpsk_t::reserved[1]

Reserved, set to zero.


Definition at line 601 of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h