RPL neighbor information.
Public Attributes#
Link-local address.
ULA/GUA address (unspecified address :: if unknown)
Neighbor type (sl_wisun_neighbor_type_t)
Remaining lifetime (Link lifetime for parents, EARO lifetime for children) in seconds.
MAC TX packet count.
MAC TX failed count.
MAC TX packet count using mode switch.
MAC TX failed count using mode switch.
MAC RX packet count.
RPL Rank value for parents (0xffff if unknown or child)
Measured ETX value if known (0xffff if unknown)
ETX to Border Router.
Number devices connected to Border Router.
Parent RSSI Out measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
Parent RSSI In measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
RSSI of the last received packet in integer dBm. */.
Indicate if the device is an LFN. 1 = LFN, 0 = FFN.
Number of PhyModeId supported.
List of phy_mode_id_count PhyModeId.
Indicate if the neighbor supports MAC mode switch.
Public Attribute Documentation#
link_local_address#
in6_addr_t sl_wisun_neighbor_info_t::link_local_address
Link-local address.
772
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
global_address#
in6_addr_t sl_wisun_neighbor_info_t::global_address
ULA/GUA address (unspecified address :: if unknown)
774
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
type#
uint32_t sl_wisun_neighbor_info_t::type
Neighbor type (sl_wisun_neighbor_type_t)
776
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
lifetime#
uint32_t sl_wisun_neighbor_info_t::lifetime
Remaining lifetime (Link lifetime for parents, EARO lifetime for children) in seconds.
778
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_count
MAC TX packet count.
780
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_failed_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_failed_count
MAC TX failed count.
782
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_ms_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_ms_count
MAC TX packet count using mode switch.
784
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_tx_ms_failed_count#
uint32_t sl_wisun_neighbor_info_t::mac_tx_ms_failed_count
MAC TX failed count using mode switch.
786
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
mac_rx_count#
uint32_t sl_wisun_neighbor_info_t::mac_rx_count
MAC RX packet count.
788
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rpl_rank#
uint16_t sl_wisun_neighbor_info_t::rpl_rank
RPL Rank value for parents (0xffff if unknown or child)
790
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
etx#
uint16_t sl_wisun_neighbor_info_t::etx
Measured ETX value if known (0xffff if unknown)
792
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
routing_cost#
uint16_t sl_wisun_neighbor_info_t::routing_cost
ETX to Border Router.
794
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
pan_size#
uint16_t sl_wisun_neighbor_info_t::pan_size
Number devices connected to Border Router.
796
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rsl_out#
uint8_t sl_wisun_neighbor_info_t::rsl_out
Parent RSSI Out measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
799
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rsl_in#
uint8_t sl_wisun_neighbor_info_t::rsl_in
Parent RSSI In measured RSSI value (0xff if unknown) Calculated using EWMA specified by Wi-SUN from range of -174 (0) to +80 (254) dBm.
802
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
rssi#
int8_t sl_wisun_neighbor_info_t::rssi
RSSI of the last received packet in integer dBm. */.
804
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
is_lfn#
uint8_t sl_wisun_neighbor_info_t::is_lfn
Indicate if the device is an LFN. 1 = LFN, 0 = FFN.
806
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
phy_mode_id_count#
uint8_t sl_wisun_neighbor_info_t::phy_mode_id_count
Number of PhyModeId supported.
808
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
phy_mode_ids#
uint8_t sl_wisun_neighbor_info_t::phy_mode_ids[SL_WISUN_MAX_PHY_MODE_ID_COUNT]
List of phy_mode_id_count PhyModeId.
810
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
is_mdr_command_capable#
uint8_t sl_wisun_neighbor_info_t::is_mdr_command_capable
Indicate if the neighbor supports MAC mode switch.
812
of file /mnt/raid/workspaces/ws.wqPNW6Hyt/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h