LFN power parameters.

Public Attributes#

uint16_t

Minimum duration of the listening window.

uint16_t

Minimum margin added to the listening window (before and after).

uint8_t

If true, the LFN wakes up only for broadcast slots containing synchronization information.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

listening_window_min_us#

uint16_t sl_wisun_lfn_params_power_t::listening_window_min_us

Minimum duration of the listening window.

Applies to both Unicast and Broadcast slots.


window_margin_min_us#

uint16_t sl_wisun_lfn_params_power_t::window_margin_min_us

Minimum margin added to the listening window (before and after).

The real margin increases with aging synchronization info.


broadcast_lts_only#

uint8_t sl_wisun_lfn_params_power_t::broadcast_lts_only

If true, the LFN wakes up only for broadcast slots containing synchronization information.

If false, the node wakes up on every LFN broadcast slot.


reserved#

uint8_t sl_wisun_lfn_params_power_t::reserved[3]

Reserved, set to zero.