FFN parameter set.

Public Attributes#

uint32_t

Version of this API.

PAN discovery parameter set.

PAN configuration parameter set.

Authentication parameter set.

RPL parameter set.

MPL parameter set.

Misc parameter set.

Public Attribute Documentation#

version#

uint32_t sl_wisun_connection_params_t::version

Version of this API.

This field allows to store the parameters in an NVM and check on reload that they are compatible with the stack if there was an update.


Definition at line 190 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

discovery#

sl_wisun_params_discovery sl_wisun_connection_params_t::discovery

PAN discovery parameter set.


Definition at line 192 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

configuration#

sl_wisun_params_configuration sl_wisun_connection_params_t::configuration

PAN configuration parameter set.


Definition at line 194 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

eapol#

sl_wisun_params_eapol sl_wisun_connection_params_t::eapol

Authentication parameter set.


Definition at line 196 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

rpl#

sl_wisun_params_rpl sl_wisun_connection_params_t::rpl

RPL parameter set.


Definition at line 198 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

mpl#

sl_wisun_params_mpl sl_wisun_connection_params_t::mpl

MPL parameter set.


Definition at line 200 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

misc#

sl_wisun_params_misc sl_wisun_connection_params_t::misc

Misc parameter set.


Definition at line 202 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h