LFN power parameters.

Public Attributes#

uint16_t

Minimum duration of the listening window.

uint16_t

Minimum margin added to the listening window (before and after).

uint8_t

If true, the LFN wakes up only for broadcast slots containing synchronization information.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

listening_window_min_us#

uint16_t sl_wisun_lfn_params_power_t::listening_window_min_us

Minimum duration of the listening window.

Applies to both Unicast and Broadcast slots.


Definition at line 101 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

window_margin_min_us#

uint16_t sl_wisun_lfn_params_power_t::window_margin_min_us

Minimum margin added to the listening window (before and after).

The real margin increases with aging synchronization info.


Definition at line 104 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

broadcast_lts_only#

uint8_t sl_wisun_lfn_params_power_t::broadcast_lts_only

If true, the LFN wakes up only for broadcast slots containing synchronization information.

If false, the node wakes up on every LFN broadcast slot.


Definition at line 108 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h

reserved#

uint8_t sl_wisun_lfn_params_power_t::reserved[3]

Reserved, set to zero.


Definition at line 110 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_lfn_params_api.h