PAN discovery parameter set.
Public Attributes#
PAN Advertisement trickle timer.
PAN Advertisement Solicit trickle timer.
uint8_t
Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.
uint8_t
If true, allow join state 1 to be skipped using cached information from the previous connection.
uint8_t
Reserved, set to zero.
Public Attribute Documentation#
trickle_pa#
sl_wisun_trickle_params_t sl_wisun_params_discovery::trickle_pa
PAN Advertisement trickle timer.
Definition at line
65
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
trickle_pas#
sl_wisun_trickle_params_t sl_wisun_params_discovery::trickle_pas
PAN Advertisement Solicit trickle timer.
Definition at line
67
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
eapol_target_min_sens#
uint8_t sl_wisun_params_discovery::eapol_target_min_sens
Minimum signal level for a node to be selected as the EAPOL target for authentication immediately after a PAN Advertisement reception.
Range from -174 (0) to +80 (254) dBm, 255 to disable feature.
Definition at line
71
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
allow_skip#
uint8_t sl_wisun_params_discovery::allow_skip
If true, allow join state 1 to be skipped using cached information from the previous connection.
Definition at line
74
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h
reserved#
uint8_t sl_wisun_params_discovery::reserved[2]
Reserved, set to zero.
Definition at line
76
of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h