MPL parameter set.

Public Attributes#

uint16_t

MPL seed set entry lifetime (seconds)

uint8_t

MPL trickle timer expirations.

uint8_t

Reserved, set to zero.

Public Attribute Documentation#

trickle#

sl_wisun_trickle_params_t sl_wisun_params_mpl::trickle

MPL trickle timer.


Definition at line 159 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

seed_set_entry_lifetime_s#

uint16_t sl_wisun_params_mpl::seed_set_entry_lifetime_s

MPL seed set entry lifetime (seconds)


Definition at line 161 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

trickle_expirations#

uint8_t sl_wisun_params_mpl::trickle_expirations

MPL trickle timer expirations.


Definition at line 163 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h

reserved#

uint8_t sl_wisun_params_mpl::reserved

Reserved, set to zero.


Definition at line 165 of file /mnt/raid/workspaces/ws.Mae4JfP9d/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_connection_params_api.h