Authentication parameter set.

Public Attributes#

uint8_t

If true, allow join state 2 to be skipped using cached credentials from the previous connection.

uint16_t

GTK_MAX_MISMATCH (minutes)

uint16_t

GTK_REQUEST_IMAX (minutes)

uint16_t

GTK_REQUEST_IMIN (minutes)

uint16_t

Initial EAPOL-Key first Tx max delay (seconds)

uint16_t

Initial EAPOL-Key first Tx min delay (seconds)

uint8_t

Initial EAPOL-Key retry limit.

uint16_t

Initial EAPOL-Key retry exponential backoff max limit (seconds)

uint16_t

Initial EAPOL-Key retry exponential backoff max (seconds)

uint16_t

Initial EAPOL-Key retry exponential backoff min (seconds)

uint16_t

LGTK_MAX_MISMATCH (minutes)

uint32_t

PMK lifetime (minutes)

uint32_t

PTK lifetime (minutes)

uint8_t

Reserved, set to zero.

uint16_t

Security protocol retry timeout (seconds)

Security protocol trickle timer.

uint8_t

Security protocol trickle timer expirations.

uint16_t

Temporary neighbor link minimum timeout (seconds)

Public Attribute Documentation#

allow_skip#

uint8_t sl_wisun_params_eapol::allow_skip

If true, allow join state 2 to be skipped using cached credentials from the previous connection.


gtk_max_mismatch_m#

uint16_t sl_wisun_params_eapol::gtk_max_mismatch_m

GTK_MAX_MISMATCH (minutes)


gtk_request_imax_m#

uint16_t sl_wisun_params_eapol::gtk_request_imax_m

GTK_REQUEST_IMAX (minutes)


gtk_request_imin_m#

uint16_t sl_wisun_params_eapol::gtk_request_imin_m

GTK_REQUEST_IMIN (minutes)


initial_key_max_s#

uint16_t sl_wisun_params_eapol::initial_key_max_s

Initial EAPOL-Key first Tx max delay (seconds)


initial_key_min_s#

uint16_t sl_wisun_params_eapol::initial_key_min_s

Initial EAPOL-Key first Tx min delay (seconds)


initial_key_retry_limit#

uint8_t sl_wisun_params_eapol::initial_key_retry_limit

Initial EAPOL-Key retry limit.


initial_key_retry_max_limit_s#

uint16_t sl_wisun_params_eapol::initial_key_retry_max_limit_s

Initial EAPOL-Key retry exponential backoff max limit (seconds)


initial_key_retry_max_s#

uint16_t sl_wisun_params_eapol::initial_key_retry_max_s

Initial EAPOL-Key retry exponential backoff max (seconds)


initial_key_retry_min_s#

uint16_t sl_wisun_params_eapol::initial_key_retry_min_s

Initial EAPOL-Key retry exponential backoff min (seconds)


lgtk_max_mismatch_m#

uint16_t sl_wisun_params_eapol::lgtk_max_mismatch_m

LGTK_MAX_MISMATCH (minutes)


pmk_lifetime_m#

uint32_t sl_wisun_params_eapol::pmk_lifetime_m

PMK lifetime (minutes)


ptk_lifetime_m#

uint32_t sl_wisun_params_eapol::ptk_lifetime_m

PTK lifetime (minutes)


reserved#

uint8_t sl_wisun_params_eapol::reserved[3]

Reserved, set to zero.


sec_prot_retry_timeout_s#

uint16_t sl_wisun_params_eapol::sec_prot_retry_timeout_s

Security protocol retry timeout (seconds)


sec_prot_trickle#

sl_wisun_trickle_params_t sl_wisun_params_eapol::sec_prot_trickle

Security protocol trickle timer.


sec_prot_trickle_expirations#

uint8_t sl_wisun_params_eapol::sec_prot_trickle_expirations

Security protocol trickle timer expirations.


temp_min_timeout_s#

uint16_t sl_wisun_params_eapol::temp_min_timeout_s

Temporary neighbor link minimum timeout (seconds)