Custom OQPSK PHY configuration.
Public Attributes#
uint32_t
Ch0 center frequency in kHz.
uint16_t
Channel spacing in kHz.
uint8_t
OFDM CRC type (sl_wisun_crc_type_t)
uint16_t
Number of channels.
uint8_t
PHY mode ID.
uint8_t
OQPSK preamble length in bits.
uint8_t
Reserved, set to zero.
Public Attribute Documentation#
ch0_frequency_khz#
uint32_t sl_wisun_phy_config_custom_oqpsk_t::ch0_frequency_khz
Ch0 center frequency in kHz.
Definition at line
589
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
channel_spacing_khz#
uint16_t sl_wisun_phy_config_custom_oqpsk_t::channel_spacing_khz
Channel spacing in kHz.
Definition at line
591
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
crc_type#
uint8_t sl_wisun_phy_config_custom_oqpsk_t::crc_type
OFDM CRC type (sl_wisun_crc_type_t)
Definition at line
597
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
number_of_channels#
uint16_t sl_wisun_phy_config_custom_oqpsk_t::number_of_channels
Number of channels.
Definition at line
593
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
phy_mode_id#
uint8_t sl_wisun_phy_config_custom_oqpsk_t::phy_mode_id
PHY mode ID.
Definition at line
595
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
preamble_length#
uint8_t sl_wisun_phy_config_custom_oqpsk_t::preamble_length
OQPSK preamble length in bits.
Definition at line
599
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
reserved#
uint8_t sl_wisun_phy_config_custom_oqpsk_t::reserved[1]
Reserved, set to zero.
Definition at line
601
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h