Custom OFDM PHY configuration.
Public Attributes#
uint32_t
Ch0 center frequency in kHz.
uint16_t
Channel spacing in kHz.
uint8_t
OFDM CRC type (sl_wisun_crc_type_t)
uint16_t
Number of channels.
uint8_t
PHY mode ID.
uint8_t
Reserved, set to zero.
uint8_t
STF length in number of symbols.
Public Attribute Documentation#
ch0_frequency_khz#
uint32_t sl_wisun_phy_config_custom_ofdm_t::ch0_frequency_khz
Ch0 center frequency in kHz.
Definition at line
571
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
channel_spacing_khz#
uint16_t sl_wisun_phy_config_custom_ofdm_t::channel_spacing_khz
Channel spacing in kHz.
Definition at line
573
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
crc_type#
uint8_t sl_wisun_phy_config_custom_ofdm_t::crc_type
OFDM CRC type (sl_wisun_crc_type_t)
Definition at line
579
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
number_of_channels#
uint16_t sl_wisun_phy_config_custom_ofdm_t::number_of_channels
Number of channels.
Definition at line
575
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
phy_mode_id#
uint8_t sl_wisun_phy_config_custom_ofdm_t::phy_mode_id
PHY mode ID.
Definition at line
577
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
reserved#
uint8_t sl_wisun_phy_config_custom_ofdm_t::reserved[1]
Reserved, set to zero.
Definition at line
583
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h
stf_length#
uint8_t sl_wisun_phy_config_custom_ofdm_t::stf_length
STF length in number of symbols.
Definition at line
581
of file /mnt/raid/workspaces/ws.TauBzA8CM/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_types.h