You are viewing documentation for version:2.12.0PDFIndication message body. Public Attributes#in6_addr_tlink_local_ipv6link local IPv6 address of the server uint32_tstateState of the Direct Connect client. Public Attribute Documentation#link_local_ipv6#in6_addr_t sl_wisun_msg_direct_connect_client_state_changed_ind_body_t::link_local_ipv6link local IPv6 address of the server state#uint32_t sl_wisun_msg_direct_connect_client_state_changed_ind_body_t::stateState of the Direct Connect client.