Indication message body.
Public Attributes#
int32_t
ID of the socket.
uint32_t
Amount of free space in the transmission buffer.
uint32_t
Status of the indication.
Public Attribute Documentation#
socket_id#
int32_t sl_wisun_msg_socket_data_sent_ind_body_t::socket_id
ID of the socket.
Definition at line
383
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
socket_space_left#
uint32_t sl_wisun_msg_socket_data_sent_ind_body_t::socket_space_left
Amount of free space in the transmission buffer.
Definition at line
385
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h
status#
uint32_t sl_wisun_msg_socket_data_sent_ind_body_t::status
Status of the indication.
Definition at line
381
of file /mnt/raid/workspaces/ws.9FtfRPWpI/overlay/gsdk/protocol/wisun/stack/inc/sl_wisun_events.h