CoAP Notify type definition.

Public Attributes#

bool(*

Condition check callback, it returns with the result of send condition (true: send, false: not send)

Packet handler callback, it returns with the built CoAP packet.

const char *

ID string.

uint32_t

Schedule time (ms)

uint32_t

Tick counter (ms)

Public Attribute Documentation#

condition_cb#

bool(* sl_wisun_coap_notify::condition_cb) (const struct sl_wisun_coap_notify *notify)

Condition check callback, it returns with the result of send condition (true: send, false: not send)


hnd_cb#

sl_wisun_coap_packet_t *(* sl_wisun_coap_notify::hnd_cb) (const struct sl_wisun_coap_notify *notify)

Packet handler callback, it returns with the built CoAP packet.


id#

const char* sl_wisun_coap_notify::id

ID string.


remote_addr#

sockaddr_in6_t sl_wisun_coap_notify::remote_addr

Remote address.


schedule_time_ms#

uint32_t sl_wisun_coap_notify::schedule_time_ms

Schedule time (ms)


tick_ms#

uint32_t sl_wisun_coap_notify::tick_ms

Tick counter (ms)