MultilevelSensor#

Modules#

_sensor_type

_sensor_read_result

_sensor_interface

_sensor_administration

Enumerations#

enum
SENSOR_NAME_AIR_TEMPERATURE = 0x00
SENSOR_NAME_GENERAL_PURPOSE
SENSOR_NAME_ILLUMINANCE
SENSOR_NAME_POWER
SENSOR_NAME_HUMIDITY
SENSOR_NAME_ACCELERATION_X
SENSOR_NAME_ACCELERATION_Y
SENSOR_NAME_ACCELERATION_Z
SENSOR_NAME_MAX_COUNT
}

Defined possible sensor types.

enum
SENSOR_READ_RESULT_SIZE_1 = 1
SENSOR_READ_RESULT_SIZE_2 = 2
SENSOR_READ_RESULT_SIZE_4 = 4
SENSOR_READ_RESULT_SIZE_END = 5
}

Defined possible sensor read size.

enum
SENSOR_READ_RESULT_PRECISION_1 = 1
SENSOR_READ_RESULT_PRECISION_2
SENSOR_READ_RESULT_PRECISION_3
SENSOR_READ_RESULT_PRECISION_END
}

Defined possible sensor read precision.

enum
SENSOR_INTERFACE_RETURN_VALUE_OK
SENSOR_INTERFACE_RETURN_VALUE_ALREADY_SET
SENSOR_INTERFACE_RETURN_VALUE_INVALID_SCALE_VALUE
SENSOR_INTERFACE_RETURN_VALUE_ERROR
SENSOR_INTERFACE_RETURN_VALUE_END
}

Defined sensor interface return values.

enum
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK
CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR
CC_MULTILEVEL_SENSOR_RETURN_VALUE_NOT_FOUND
CC_MULTILEVEL_SENSOR_RETURN_VALUE_ALREADY_REGISTRATED
CC_MULTILEVEL_SENSOR_RETURN_VALUE_REGISTRATION_LIMIT_REACHED
CC_MULTILEVEL_SENSOR_RETURN_VALUE_END
}

Defined Multilevel Sensor return values.

Typedefs#

typedef enum sensor_name

Defined possible sensor types.

typedef struct _sensor_type

Structure that holds the attributes of a sensor type.

typedef struct _sensor_interface

Structure that holds a read result from the read interface.

typedef struct _sensor_administration

Structure that administrate all of the registered sensors.

Functions#

void

This function will report the registered sensor's measured datas to the Lifeline group.

void

Calls the init function for all of the registered sensor interfaces.

uint8_t
cc_multilevel_sensor_check_scale(const sensor_interface_t *i_interface, uint8_t i_scale)

Checks if the wanted scale is a legal one for an interface.

Checks if the wanted sensor type has a registered interface or not.

cc_multilevel_sensor_registration(sensor_interface_t *i_new_sensor)

Registers an interface to a specific sensor type.

cc_multilevel_sensor_get_supported_sensors(uint8_t *o_supported_sensor_buffer)

Fills an input buffer with flags where each flag represents a supported sensor.

cc_multilevel_sensor_get_supported_scale(uint8_t sensor_type_value, uint8_t *o_supported_scale)

Fills an input buffer with flags where each flag represents a supported scale.

cc_multilevel_sensor_get_interface(uint8_t sensor_type_value, sensor_interface_t **o_interface)

Getter function for a sensor type's interface.

cc_multilevel_sensor_get_default_sensor_type(uint8_t *o_default_sensor_type)

Gets the default sensor type value.

cc_multilevel_sensor_init_iterator(sensor_interface_iterator_t **i_iterator)

Initialize an iterator struct for the registered sensor interfaces.

void
cc_multilevel_sensor_next_iterator(sensor_interface_iterator_t **i_iterator)

Moves the iterator reference forward to the next registered interface, if the current is the last one then NULL If there is any registered interface the iterator will be NULL.

uint8_t

Returns the number of registered sensor interfaces.

void

Removes all of the registered sensor interfaces from the administration.

cc_multilevel_sensor_get_sensor_type(sensor_name_t i_sensor_name)

Returns a sensor_type_t struct from the sensor_types config table.

cc_multilevel_sensor_init_interface(sensor_interface_t *i_instance, sensor_name_t i_name)

Initialize a sensor interface instance.

cc_multilevel_sensor_add_supported_scale_interface(sensor_interface_t *i_instance, uint8_t i_scale)

Adds a new scale to an existing interface.

Macros#

#define
MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SEC (MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MIN*60)
#define
MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MS (MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SEC*1000)
#define
#define
#define
SENSOR_SCALE_BTU_H 0x01 /*Btu/h*/
#define
#define
#define

Structure that holds a read result from the read interface.

Enumeration Documentation#

sensor_name#

sensor_name

Defined possible sensor types.

Enumerator
SENSOR_NAME_AIR_TEMPERATURE
SENSOR_NAME_GENERAL_PURPOSE
SENSOR_NAME_ILLUMINANCE
SENSOR_NAME_POWER
SENSOR_NAME_HUMIDITY
SENSOR_NAME_ACCELERATION_X
SENSOR_NAME_ACCELERATION_Y
SENSOR_NAME_ACCELERATION_Z
SENSOR_NAME_MAX_COUNT

Definition at line 51 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_read_result_size_t#

sensor_read_result_size_t

Defined possible sensor read size.

Enumerator
SENSOR_READ_RESULT_SIZE_1
SENSOR_READ_RESULT_SIZE_2
SENSOR_READ_RESULT_SIZE_4
SENSOR_READ_RESULT_SIZE_END

Definition at line 76 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_read_result_precision#

sensor_read_result_precision

Defined possible sensor read precision.

Enumerator
SENSOR_READ_RESULT_PRECISION_1
SENSOR_READ_RESULT_PRECISION_2
SENSOR_READ_RESULT_PRECISION_3
SENSOR_READ_RESULT_PRECISION_END

Definition at line 86 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_interface_return_value_t#

sensor_interface_return_value_t

Defined sensor interface return values.

Enumerator
SENSOR_INTERFACE_RETURN_VALUE_OK
SENSOR_INTERFACE_RETURN_VALUE_ALREADY_SET
SENSOR_INTERFACE_RETURN_VALUE_INVALID_SCALE_VALUE
SENSOR_INTERFACE_RETURN_VALUE_ERROR
SENSOR_INTERFACE_RETURN_VALUE_END

Definition at line 117 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

cc_multilevel_sensor_return_value#

cc_multilevel_sensor_return_value

Defined Multilevel Sensor return values.

Enumerator
CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK
CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR
CC_MULTILEVEL_SENSOR_RETURN_VALUE_NOT_FOUND
CC_MULTILEVEL_SENSOR_RETURN_VALUE_ALREADY_REGISTRATED
CC_MULTILEVEL_SENSOR_RETURN_VALUE_REGISTRATION_LIMIT_REACHED
CC_MULTILEVEL_SENSOR_RETURN_VALUE_END

Definition at line 128 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

Typedef Documentation#

sensor_name_t#

typedef enum sensor_name sensor_name_t

Defined possible sensor types.


Definition at line 61 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_type_t#

typedef struct _sensor_type sensor_type_t

Structure that holds the attributes of a sensor type.


Definition at line 71 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_read_result_t#

typedef struct _sensor_read_result sensor_read_result_t

Definition at line 101 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_interface_t#

typedef struct _sensor_interface sensor_interface_t

Structure that holds a read result from the read interface.


Definition at line 112 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_interface_iterator_t#

typedef struct _sensor_interface sensor_interface_iterator_t

Definition at line 112 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

sensor_administration_t#

typedef struct _sensor_administration sensor_administration_t

Structure that administrate all of the registered sensors.


Definition at line 144 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

Function Documentation#

cc_multilevel_sensor_send_sensor_data#

void cc_multilevel_sensor_send_sensor_data (void )

This function will report the registered sensor's measured datas to the Lifeline group.

Parameters
N/A

Definition at line 49 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/inc/CC_MultilevelSensor_Support.h

cc_multilevel_sensor_config_register_instances#

void cc_multilevel_sensor_config_register_instances (void )
Parameters
N/A

Definition at line 21 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/cc_multilevel_sensor_config_api.h

cc_multilevel_sensor_init_all_sensor#

void cc_multilevel_sensor_init_all_sensor (void )

Calls the init function for all of the registered sensor interfaces.

Parameters
N/A

Definition at line 48 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_check_scale#

uint8_t cc_multilevel_sensor_check_scale (const sensor_interface_t * i_interface, uint8_t i_scale)

Checks if the wanted scale is a legal one for an interface.

Parameters
[in]i_interface

Pointer to an existing sensor interface

[in]i_scale

Scale value to check

If the scale is not set the function will return with the first available scale. The function will iterate from bit 0 to 7 to look for the first scale which is supported. That will be the default scale. Returns

  • a usable scale value, if the input i_scale is valid that will be return, else the default one.


Definition at line 60 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_check_sensor_type_registered#

cc_multilevel_sensor_return_value cc_multilevel_sensor_check_sensor_type_registered (uint8_t sensor_type_value)

Checks if the wanted sensor type has a registered interface or not.

Parameters
[in]sensor_type_value

Sensor type value to check, this is the value in sensor_type_t struct's value

Returns

  • CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_NOT_FOUND.


Definition at line 68 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_registration#

cc_multilevel_sensor_return_value cc_multilevel_sensor_registration (sensor_interface_t * i_new_sensor)

Registers an interface to a specific sensor type.

Parameters
[in]i_new_sensor

Pointer to a filled sensor interface struct

The number of registered sensor types is maximized with REGISTERED_SENSOR_NUMBER_LIMIT Returns

  • CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor.


Definition at line 77 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_get_supported_sensors#

cc_multilevel_sensor_return_value cc_multilevel_sensor_get_supported_sensors (uint8_t * o_supported_sensor_buffer)

Fills an input buffer with flags where each flag represents a supported sensor.

Parameters
[out]o_supported_sensor_buffer

Pointer to a buffer where the supported sensors' are represented as flags in a byte array. The position of each flag is calculated based on SDS13812. The buffer must be 11 byte long at least.

Returns

  • CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if success, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR.


Definition at line 86 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_get_supported_scale#

cc_multilevel_sensor_return_value cc_multilevel_sensor_get_supported_scale (uint8_t sensor_type_value, uint8_t * o_supported_scale)

Fills an input buffer with flags where each flag represents a supported scale.

Parameters
[in]sensor_type_value

Sensor type value to check, this is the value in sensor_type_t struct's value

[out]o_supported_scale

Pointer to a buffer where the supported scales will be represented for a sensor type

Returns

  • CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor.


Definition at line 95 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_get_interface#

cc_multilevel_sensor_return_value cc_multilevel_sensor_get_interface (uint8_t sensor_type_value, sensor_interface_t ** o_interface)

Getter function for a sensor type's interface.

Parameters
[in]sensor_type_value

Sensor type value to check, this is the value in sensor_type_t struct's value

[out]o_interface

This is a double pointer which will hold an interface reference

Returns

  • CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if interface is registered for a sensor, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_NOT_FOUND.


Definition at line 104 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_get_default_sensor_type#

cc_multilevel_sensor_return_value cc_multilevel_sensor_get_default_sensor_type (uint8_t * o_default_sensor_type)

Gets the default sensor type value.

Parameters
[in]o_default_sensor_type

Pointer to a byte buffer which will hold the default sensor type value

Basically the first registered sensor interface' type is the default one. Returns

  • CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if there is any registered interface, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR.


Definition at line 112 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_init_iterator#

cc_multilevel_sensor_return_value cc_multilevel_sensor_init_iterator (sensor_interface_iterator_t ** i_iterator)

Initialize an iterator struct for the registered sensor interfaces.

Parameters
[out]i_iterator

This is a double pointer which will hold an interface reference to the first registered interface

If there is any registered interface the iterator will be NULL. Returns

  • CC_MULTILEVEL_SENSOR_RETURN_VALUE_OK if success, else CC_MULTILEVEL_SENSOR_RETURN_VALUE_ERROR..


Definition at line 121 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_next_iterator#

void cc_multilevel_sensor_next_iterator (sensor_interface_iterator_t ** i_iterator)

Moves the iterator reference forward to the next registered interface, if the current is the last one then NULL If there is any registered interface the iterator will be NULL.

Parameters
[out]i_iterator

This is a double pointer which will hold an interface reference


Definition at line 129 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_get_number_of_registered_sensors#

uint8_t cc_multilevel_sensor_get_number_of_registered_sensors (void )

Returns the number of registered sensor interfaces.

Parameters
N/A

Returns

  • Number of registered sensor interfaces.


Definition at line 136 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_reset_administration#

void cc_multilevel_sensor_reset_administration (void )

Removes all of the registered sensor interfaces from the administration.

Parameters
N/A

Definition at line 142 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandler.h

cc_multilevel_sensor_get_sensor_type#

const sensor_type_t * cc_multilevel_sensor_get_sensor_type (sensor_name_t i_sensor_name)

Returns a sensor_type_t struct from the sensor_types config table.

Parameters
[in]i_sensor_name

The name of the sensor type, the sensor type attributes' reference will be look for based on this value

Returns

  • sensor_type_t struct which includes the type attributes.


Definition at line 161 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

cc_multilevel_sensor_init_interface#

sensor_interface_return_value_t cc_multilevel_sensor_init_interface (sensor_interface_t * i_instance, sensor_name_t i_name)

Initialize a sensor interface instance.

Parameters
[in]i_instance

Pointer to an existing sensor interface to init

[in]i_name

The name of the sensor type, the sensor type attributes' reference will be look for based on this value

Sets the whole struct to zero and sets the reference to the appropiate sensor_type_t struct. Returns

  • Status of the initialization.


Definition at line 173 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

cc_multilevel_sensor_add_supported_scale_interface#

sensor_interface_return_value_t cc_multilevel_sensor_add_supported_scale_interface (sensor_interface_t * i_instance, uint8_t i_scale)

Adds a new scale to an existing interface.

Parameters
[in]i_instance

Pointer to an existing sensor interface which the new scale will be registered to

[in]i_scale

The new scale which will be registered

Supported scales must be set by this function during initialization. Returns

  • Status of the new scale value registration.


Definition at line 183 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

Macro Definition Documentation#

MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SEC#

#define MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SEC
Value:
(MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MIN*60)

Definition at line 35 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/inc/CC_MultilevelSensor_Support.h

MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MS#

#define MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_MS
Value:
(MULTILEVEL_SENSOR_DEFAULT_AUTOREPORT_PEDIOD_SEC*1000)

Definition at line 36 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/inc/CC_MultilevelSensor_Support.h

SENSOR_SCALE_DEFAULT#

#define SENSOR_SCALE_DEFAULT
Value:
0x00

Definition at line 37 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_CELSIUS#

#define SENSOR_SCALE_CELSIUS
Value:
0x00

Definition at line 38 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_FAHRENHEIT#

#define SENSOR_SCALE_FAHRENHEIT
Value:
0x01

Definition at line 39 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_PERCENTAGE#

#define SENSOR_SCALE_PERCENTAGE
Value:
0x00

Definition at line 40 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_DIMENSIONLESS#

#define SENSOR_SCALE_DIMENSIONLESS
Value:
0x01

Definition at line 41 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_LUX#

#define SENSOR_SCALE_LUX
Value:
0x01

Definition at line 42 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_WATT#

#define SENSOR_SCALE_WATT
Value:
0x00

Definition at line 43 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_BTU_H#

#define SENSOR_SCALE_BTU_H
Value:
0x01 /*Btu/h*/

Definition at line 44 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_ABSOLUTE_HUMIDITY#

#define SENSOR_SCALE_ABSOLUTE_HUMIDITY
Value:
0x01 /*g/m3*/

Definition at line 45 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SENSOR_SCALE_METER_SQUARE_SECOND#

#define SENSOR_SCALE_METER_SQUARE_SECOND
Value:
0x00 /*m/s^2*/

Definition at line 46 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h

SLI_MAX_RAW_RESULT_BYTES#

#define SLI_MAX_RAW_RESULT_BYTES
Value:
4

Structure that holds a read result from the read interface.


Definition at line 96 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/MultilevelSensor/src/CC_MultilevelSensor_SensorHandlerTypes.h