Notification#

Command Class Notification enables a device to send notifications like "smoke detected" or "window opened".

CC Notification is typically used in sensor applications because it supports many different notification/sensor types.

CC Notification requires at least one notification to be configured by implementing the functions declared in cc_notification_config_api.h. Simplicity Studio / SLC generates this configuration automatically based on user configuration in *.cc_config files.

This command class offers one single API function to be used by the application:

The specification of CC Notification can be found in https://github.com/Z-Wave-Alliance/AWG/blob/main/source/application_command_classes/command_class_definitions/notification_command_class_version_3-8.rst.

Modules#

s_CC_notification_data_t_

Configuration of CC Notification

Storage for CC Notification

Enumerations#

enum
NOTIFICATION_EVENT_NO_EVENT
NOTIFICATION_EVENT_UNKNOWN_EVENT = 0xFE
}

General purpose notification event.

enum
NOTIFICATION_TYPE_NONE
NOTIFICATION_TYPE_SMOKE_ALARM = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_SMOKE_ALARM)
NOTIFICATION_TYPE_CO_ALARM = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_CO_ALARM)
NOTIFICATION_TYPE_CO2_ALARM = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_CO2_ALARM)
NOTIFICATION_TYPE_HEAT_ALARM = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_HEAT_ALARM)
NOTIFICATION_TYPE_WATER_ALARM = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_WATER_ALARM)
NOTIFICATION_TYPE_ACCESS_CONTROL = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_ACCESS_CONTROL)
NOTIFICATION_TYPE_HOME_SECURITY = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_HOME_SECURITY)
NOTIFICATION_TYPE_POWER_MANAGEMENT = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_POWER_MANAGEMENT)
NOTIFICATION_TYPE_SYSTEM = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_SYSTEM)
NOTIFICATION_TYPE_EMERGENCY_ALARM = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_EMERGENCY_ALARM)
NOTIFICATION_TYPE_CLOCK = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_CLOCK)
NOTIFICATION_TYPE_MULTIDEVICE = (0xFF & ICON_TYPE_SPECIFIC_SENSOR_NOTIFICATION_MULTIDEVICE)
}

Notification type (8 bit).

Typedefs#

Struct used to pass operational data to TSE module.

Functions#

CC_Notification_TriggerAndTransmit(uint8_t index, uint8_t notificationEvent, uint8_t *pEvPar, uint8_t evParLen, void(*pCallback)(TRANSMISSION_RESULT *pTransmissionResult), bool tse)

Triggers notification event and sends it to dedicated Agi profile.

Macros#

#define

the maximum length of the notification bitmask array

Enumeration Documentation#

NOTIFICATION_EVENT#

NOTIFICATION_EVENT

General purpose notification event.

Enumerator
NOTIFICATION_EVENT_NO_EVENT
NOTIFICATION_EVENT_UNKNOWN_EVENT

Definition at line 56 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h

notification_type_t#

notification_type_t

Notification type (8 bit).

Enumerator
NOTIFICATION_TYPE_NONE
NOTIFICATION_TYPE_SMOKE_ALARM
NOTIFICATION_TYPE_CO_ALARM
NOTIFICATION_TYPE_CO2_ALARM
NOTIFICATION_TYPE_HEAT_ALARM
NOTIFICATION_TYPE_WATER_ALARM
NOTIFICATION_TYPE_ACCESS_CONTROL
NOTIFICATION_TYPE_HOME_SECURITY
NOTIFICATION_TYPE_POWER_MANAGEMENT
NOTIFICATION_TYPE_SYSTEM
NOTIFICATION_TYPE_EMERGENCY_ALARM
NOTIFICATION_TYPE_CLOCK
NOTIFICATION_TYPE_MULTIDEVICE

Definition at line 21 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/cc_notification_types.h

Typedef Documentation#

s_CC_notification_data_t#

typedef struct s_CC_notification_data_t_ s_CC_notification_data_t

Struct used to pass operational data to TSE module.


Definition at line 71 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h

Function Documentation#

CC_Notification_TriggerAndTransmit#

JOB_STATUS CC_Notification_TriggerAndTransmit (uint8_t index, uint8_t notificationEvent, uint8_t * pEvPar, uint8_t evParLen, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCallback, bool tse)

Triggers notification event and sends it to dedicated Agi profile.

Parameters
[in]index

notification index.

[in]notificationEvent

Event triggered.

[in]pEvPar

point to event parameters.

[in]evParLen

length of event parameters.

[out]pCallback

callback function returning state on job

[in]tse

True of false, depending if TSE should be triggered, or not

Returns

  • JOB_STATUS


Definition at line 83 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h

Macro Definition Documentation#

NOTIFICATION_BITMASK_ARRAY_LENGTH#

#define NOTIFICATION_BITMASK_ARRAY_LENGTH
Value:
32

the maximum length of the notification bitmask array


Definition at line 51 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Notification/inc/CC_Notification.h