UserCode#
Modules#
Enumerations#
Typedefs#
Struct used to pass operational data to TSE module.
Functions#
The User Code Set Command used to set a User Code in the device.
The User Code Get ID.
The User Code Report Command can be used by e.g.
The Users Number Report Command used to report the maximum number of USER CODES the given node supports.
Resets the data used by the command class.
Set the user code to a new value.
Send a Command Class User code support report.
Macros#
Minimum length of a user code as defined in SDS12652.
Maximum length of a user code as defined in SDS12652.
Enumeration Documentation#
user_id_status_t#
user_id_status_t
User ID Status.#
The User ID Status field indicates the state of the User Identifier. All other values not mentioned in below list are reserved for future implementation.
Hex | Description |
|---|---|
00 | Available (not set) |
01 | Occupied |
02 | Reserved by administrator |
FE | Status not available |
| Enumerator | |
|---|---|
| USER_ID_AVAILABLE | Available (not set) |
| USER_ID_OCCUPIED | Occupied. |
| USER_ID_RESERVED | Reserved by administrator. |
| USER_ID_NO_STATUS | Status not available. |
Typedef Documentation#
s_CC_userCode_data_t#
typedef struct s_CC_userCode_data_t_ s_CC_userCode_data_t
Struct used to pass operational data to TSE module.
Function Documentation#
CC_UserCode_Write#
bool CC_UserCode_Write (uint8_t identifier, SUserCode * userCodeData)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | identifier | |
| SUserCode * | N/A | userCodeData |
CC_UserCode_Read#
bool CC_UserCode_Read (uint8_t identifier, SUserCode * userCodeData)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | identifier | |
| SUserCode * | N/A | userCodeData |
CC_UserCode_Set_handler#
e_cmd_handler_return_code_t CC_UserCode_Set_handler (uint8_t identifier, USER_ID_STATUS id, uint8_t * pUserCode, uint8_t len, uint16_t modifierNodeId)
The User Code Set Command used to set a User Code in the device.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | identifier | User Identifier. |
| USER_ID_STATUS | [in] | id | user Id status. |
| uint8_t * | [in] | pUserCode | pointer to UserCode data. |
| uint8_t | [in] | len | UserCode data. |
| uint16_t | [in] | modifierNodeId | Node ID of the requesting node. |
Returns
command handler return code
CC_UserCode_getId_handler#
bool CC_UserCode_getId_handler (uint8_t identifier, USER_ID_STATUS * pId, uint8_t endpoint)
The User Code Get ID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | identifier | User Identifier. |
| USER_ID_STATUS * | [out] | pId | pointer to return Id. |
| uint8_t | [in] | endpoint | is the destination endpoint |
Returns
status valid boolean.
CC_UserCode_Report_handler#
bool CC_UserCode_Report_handler (uint8_t identifier, uint8_t * pUserCode, size_t * pLen, uint8_t endpoint)
The User Code Report Command can be used by e.g.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | identifier | User Identifier. |
| uint8_t * | [out] | pUserCode | pointer to UserCode data. |
| size_t * | [out] | pLen | length UserCode data. |
| uint8_t | [in] | endpoint | is the destination endpoint |
a door lock device to send a report either unsolicited or requested by the User Code Get Command. Returns
status valid boolean.
CC_UserCode_UsersNumberReport_handler#
uint8_t CC_UserCode_UsersNumberReport_handler (uint8_t endpoint)
The Users Number Report Command used to report the maximum number of USER CODES the given node supports.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | endpoint | is the destination endpoint |
The Users Number Report Command can be send requested by the Users Number Get Command. Returns
maximum number of USER CODES.
CC_UserCode_reset_data#
void CC_UserCode_reset_data (void )
Resets the data used by the command class.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
CC_UserCode_set_usercode#
void CC_UserCode_set_usercode (char * new_user_code)
Set the user code to a new value.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| char * | [in] | new_user_code | The new user code, must be under the length of USERCODE_MAX_LEN |
CC_UserCode_SupportReport#
JOB_STATUS CC_UserCode_SupportReport (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, uint8_t userIdentifier, uint8_t userIdStatus, uint8_t * pUserCode, uint8_t userCodeLen, void(*)(TRANSMISSION_RESULT *pTransmissionResult) pCallback)
Send a Command Class User code support report.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| AGI_PROFILE * | [in] | pProfile | pointer to AGI profile |
| uint8_t | [in] | sourceEndpoint | source endpoint |
| uint8_t | [in] | userIdentifier | user identifier |
| uint8_t | [in] | userIdStatus | user Id status |
| uint8_t * | [in] | pUserCode | user code |
| uint8_t | [in] | userCodeLen | length of user code |
| void(*)(TRANSMISSION_RESULT *pTransmissionResult) | [out] | pCallback | callback function returning status destination node receive job. |
Returns
status on the job.
CC_UserCode_Validate#
bool CC_UserCode_Validate (uint8_t identifier, const uint8_t * pCode, uint8_t len)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | identifier | |
| const uint8_t * | N/A | pCode | |
| uint8_t | N/A | len |