Basic#

Functions#

CC_Basic_Report_tx(AGI_PROFILE *pProfile, uint8_t sourceEndpoint, uint8_t bValue, ZAF_TX_Callback_t callback)

Send unsolicited command class Basic report.

CC_Basic_Set_tx(agi_profile_t const *const p_profile, const uint8_t source_endpoint, const uint8_t value, const bool use_supervision, ZAF_TX_Callback_t callback)

Sends an unsolicited Basic Set command.

Function Documentation#

CC_Basic_Report_tx#

JOB_STATUS CC_Basic_Report_tx (AGI_PROFILE * pProfile, uint8_t sourceEndpoint, uint8_t bValue, ZAF_TX_Callback_t callback)

Send unsolicited command class Basic report.

Parameters
[in]pProfile

pointer to AGI profile

[in]sourceEndpoint

source endpoint

[in]bValue

Basic Report value

[out]callback

callback function pointer returning status on job. Can be initialized to NULL.

Returns

  • status of the job of type JOB_STATUS


Definition at line 27 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Basic/inc/CC_Basic.h

CC_Basic_Set_tx#

zaf_job_status_t CC_Basic_Set_tx (agi_profile_t const *const p_profile, const uint8_t source_endpoint, const uint8_t value, const bool use_supervision, ZAF_TX_Callback_t callback)

Sends an unsolicited Basic Set command.

Parameters
[in]p_profile

Pointer to an AGI profile defined in the configuration of CC AGI.

[in]source_endpoint

Source endpoint if the sending device use endpoints. Otherwise 0.

[in]value

Value as defined in the specification of the command.

[in]use_supervision

Use Supervision for transmission of this Basic Set.

[out]callback

Callback function pointer giving a result of the transmission.

Returns

  • Status on whether the transmission could be initiated.


Definition at line 43 of file /mnt/raid/workspaces/ws.eV40Coy1M/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Basic/inc/CC_Basic.h