Struct used to pass operational data to TSE module.
See ZAF_TSE_Trigger() for more information.
Receive options MUST be the first element as TSE relies on the receive options.
Public Attribute Documentation#
rxOptions#
RECEIVE_OPTIONS_TYPE_EX s_CC_indicator_data_t_::rxOptions
rxOptions
Definition at line
42
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Indicator/inc/CC_Indicator.h
indicatorId#
uint8_t s_CC_indicator_data_t_::indicatorId
Indicator Id.
Definition at line
43
of file /mnt/raid/workspaces/ws.ZFSvPe7ik/overlay/gsdk/protocol/z-wave/ZAF/CommandClasses/Indicator/inc/CC_Indicator.h