You are viewing documentation for version:
PDFDefines the different types that a value can take, e.g.
uint8_t, int16_t, etc.
Public Attribute Documentation#
as_uint32#
uint32_t cc_config_parameter_value_t::as_uint32
as_uint16#
uint16_t cc_config_parameter_value_t::as_uint16
as_uint8#
uint8_t cc_config_parameter_value_t::as_uint8
as_int32#
int32_t cc_config_parameter_value_t::as_int32
as_int16#
int16_t cc_config_parameter_value_t::as_int16
as_int8#
int8_t cc_config_parameter_value_t::as_int8
as_uint8_array#
uint8_t cc_config_parameter_value_t::as_uint8_array[4]