Public Attributes#
< Frame header info
Command sender Node ID.
Frame destination ID, only valid when frame is not Multicast.
Security key frame was received with.
CommunicationProfile used on receive.
Channel on which frame was received is a Z-Wave Long Range channel.
Transmit power used by the source to transmit the frame.
Noise floor measured by the source node before transmitting.
Public Attribute Documentation#
rxStatus#
uint8_t _RECEIVE_OPTIONS_TYPE::rxStatus
< Frame header info
Command sender Home ID
163
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
homeId#
union _RECEIVE_OPTIONS_TYPE::@2 _RECEIVE_OPTIONS_TYPE::homeId
Command sender Node ID.
169
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
sourceNode#
node_id_t _RECEIVE_OPTIONS_TYPE::sourceNode
Frame destination ID, only valid when frame is not Multicast.
170
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
destNode#
node_id_t _RECEIVE_OPTIONS_TYPE::destNode
Average RSSI val in dBm as defined in RSSI feedback constants above.
172
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
rxRSSIVal#
signed char _RECEIVE_OPTIONS_TYPE::rxRSSIVal
Security key frame was received with.
174
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
securityKey#
enum SECURITY_KEY _RECEIVE_OPTIONS_TYPE::securityKey
CommunicationProfile used on receive.
176
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
rxSpeed#
uint8_t _RECEIVE_OPTIONS_TYPE::rxSpeed
Channel on which frame was received is a Z-Wave Long Range channel.
178
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
isLongRangeChannel#
bool _RECEIVE_OPTIONS_TYPE::isLongRangeChannel
Transmit power used by the source to transmit the frame.
180
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bSourceTxPower#
int8_t _RECEIVE_OPTIONS_TYPE::bSourceTxPower
Noise floor measured by the source node before transmitting.
182
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h
bSourceNoiseFloor#
int8_t _RECEIVE_OPTIONS_TYPE::bSourceNoiseFloor
184
of file /mnt/raid/workspaces/ws.6QOxxjIBR/overlay/gsdk/protocol/z-wave/ZWave/API/ZW_transport_api.h