Transmit Options#

Transmit frame option flags.

Macros#

#define

Request acknowledge from destination node.

#define

Rransmit at low output power level (1/3 of normal RF range)

#define

The multicast frame should be send as a broadcast.

#define

Request retransmission via repeater nodes.

#define

Do not use response route - Even if available.

#define

Use explore frame if needed.

#define

Urgent frame - go to the front of the queue.

Macro Definition Documentation#

TRANSMIT_OPTION_ACK#

#define TRANSMIT_OPTION_ACK
Value:
0x01

Request acknowledge from destination node.


TRANSMIT_OPTION_LOW_POWER#

#define TRANSMIT_OPTION_LOW_POWER
Value:
0x02

Rransmit at low output power level (1/3 of normal RF range)


TRANSMIT_OPTION_MULTICAST_AS_BROADCAST#

#define TRANSMIT_OPTION_MULTICAST_AS_BROADCAST
Value:
0x02

The multicast frame should be send as a broadcast.


TRANSMIT_OPTION_AUTO_ROUTE#

#define TRANSMIT_OPTION_AUTO_ROUTE
Value:
0x04

Request retransmission via repeater nodes.


TRANSMIT_OPTION_NO_ROUTE#

#define TRANSMIT_OPTION_NO_ROUTE
Value:
0x10

Do not use response route - Even if available.


TRANSMIT_OPTION_EXPLORE#

#define TRANSMIT_OPTION_EXPLORE
Value:
0x20

Use explore frame if needed.


TRANSMIT_OPTION_URGENT#

#define TRANSMIT_OPTION_URGENT
Value:
0x08

Urgent frame - go to the front of the queue.