Public Attributes#
void(*
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
Routing slave to recieve route.
uint8_t
Destination of route (if 0 destination will be self). Destination can be a SUC.
uint8_t
Route to be assigned as priority route - set to zeroes to NOT supply a priority route (recommended)
uint8_t
Public Attribute Documentation#
ReturnRouteReceiverNodeId#
node_id_t SAssignReturnRoute::ReturnRouteReceiverNodeId
Placeholder for callback function Will be returned with transmit status Allows application to recognize frames.
RouteDestinationNodeId#
node_id_t SAssignReturnRoute::RouteDestinationNodeId
Routing slave to recieve route.
aPriorityRouteRepeaters#
uint8_t SAssignReturnRoute::aPriorityRouteRepeaters[4]
Destination of route (if 0 destination will be self). Destination can be a SUC.
PriorityRouteSpeed#
uint8_t SAssignReturnRoute::PriorityRouteSpeed
Route to be assigned as priority route - set to zeroes to NOT supply a priority route (recommended)