Button Interface Callbacks
These callbacks are contributed by the Button Interface plugin.
Functions#
Called when Button 0 is pressed short.
Called when Button 1 is pressed short.
Called when Button 0 is pressed long.
Called when Button 1 is pressed long.
Called while Button 0 is pressed.
Called while Button 1 is pressed.
Called when Button 0 goes low.
Called when Button 0 goes high.
Called when Button 1 goes low.
Called when Button 1 goes high.
Function Documentation#
emberAfPluginButtonInterfaceButton0PressedShortCallback
void emberAfPluginButtonInterfaceButton0PressedShortCallback (uint16_t timePressedMs)
Called when Button 0 is pressed short.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | N/A | timePressedMs | Time (in ms) button 0 was pressed short | 
emberAfPluginButtonInterfaceButton1PressedShortCallback
void emberAfPluginButtonInterfaceButton1PressedShortCallback (uint16_t timePressedMs)
Called when Button 1 is pressed short.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | N/A | timePressedMs | Time (in ms) button 1 was pressed short | 
emberAfPluginButtonInterfaceButton0PressedLongCallback
void emberAfPluginButtonInterfaceButton0PressedLongCallback (uint16_t timePressedMs, bool pressedAtReset)
Called when Button 0 is pressed long.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | N/A | timePressedMs | Amount of time button 0 was pressed. | 
| bool | N/A | pressedAtReset | Was the button pressed at startup. | 
emberAfPluginButtonInterfaceButton1PressedLongCallback
void emberAfPluginButtonInterfaceButton1PressedLongCallback (uint16_t timePressedMs, bool pressedAtReset)
Called when Button 1 is pressed long.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| uint16_t | N/A | timePressedMs | Amount of time button 1 was pressed. | 
| bool | N/A | pressedAtReset | Was the button pressed at startup. | 
emberAfPluginButtonInterfaceButton0PressingCallback
void emberAfPluginButtonInterfaceButton0PressingCallback (void )
Called while Button 0 is pressed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function is periodically called when button 0 is being pressed.
emberAfPluginButtonInterfaceButton1PressingCallback
void emberAfPluginButtonInterfaceButton1PressingCallback (void )
Called while Button 1 is pressed.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function is periodically called when button 1 is being pressed.
emberAfPluginButtonInterfaceButton0LowCallback
void emberAfPluginButtonInterfaceButton0LowCallback (void )
Called when Button 0 goes low.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function is called when the GPIO tied to button zero goes low
emberAfPluginButtonInterfaceButton0HighCallback
void emberAfPluginButtonInterfaceButton0HighCallback (void )
Called when Button 0 goes high.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function is called when the GPIO tied to button zero goes high
emberAfPluginButtonInterfaceButton1LowCallback
void emberAfPluginButtonInterfaceButton1LowCallback (void )
Called when Button 1 goes low.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function is called when the GPIO tied to button one goes low
emberAfPluginButtonInterfaceButton1HighCallback
void emberAfPluginButtonInterfaceButton1HighCallback (void )
Called when Button 1 goes high.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
This function is called when the GPIO tied to button one goes high