The internal representation of a proxy or sink table entry.
Public Attribute Documentation#
status#
EmberGpProxyTableEntryStatus EmberGpProxyTableEntry::status
Internal status. Defines if the entry is unused or used as a proxy entry
Definition at line
194
of file stack/include/gp-types.h
options#
uint32_t EmberGpProxyTableEntry::options
The tunneling options (this contains both options and extendedOptions from the spec)
Definition at line
198
of file stack/include/gp-types.h
gpd#
EmberGpAddress EmberGpProxyTableEntry::gpd
The addressing info of the GPD
Definition at line
202
of file stack/include/gp-types.h
assignedAlias#
EmberNodeId EmberGpProxyTableEntry::assignedAlias
The assigned alias for the GPD
Definition at line
206
of file stack/include/gp-types.h
securityOptions#
uint8_t EmberGpProxyTableEntry::securityOptions
The security options field
Definition at line
210
of file stack/include/gp-types.h
gpdSecurityFrameCounter#
EmberGpSecurityFrameCounter EmberGpProxyTableEntry::gpdSecurityFrameCounter
The SFC of the GPD
Definition at line
214
of file stack/include/gp-types.h
gpdKey#
EmberKeyData EmberGpProxyTableEntry::gpdKey
The key
Definition at line
218
of file stack/include/gp-types.h
sinkList#
EmberGpSinkListEntry EmberGpProxyTableEntry::sinkList[GP_SINK_LIST_ENTRIES]
The list of sinks (hardcoded to 2 which is the spec minimum) (maybe we should indirect this?)
Definition at line
222
of file stack/include/gp-types.h
groupcastRadius#
uint8_t EmberGpProxyTableEntry::groupcastRadius
The groupcast radius
Definition at line
226
of file stack/include/gp-types.h
searchCounter#
uint8_t EmberGpProxyTableEntry::searchCounter
The search counter
Definition at line
230
of file stack/include/gp-types.h