The internal representation of a proxy or sink table entry.
Public Attribute Documentation#
status#
EmberGpSinkTableEntryStatus EmberGpSinkTableEntry::status
Internal status. Defines if the entry is unused or used as a sink table entry
options#
uint16_t EmberGpSinkTableEntry::options
The tunneling options (this contains both options and extendedOptions from the spec)
sinkList#
EmberGpSinkListEntry EmberGpSinkTableEntry::sinkList[GP_SINK_LIST_ENTRIES]
The list of sinks (hardcoded to 2 which is the spec minimum) (maybe we should indirect this?)
gpdSecurityFrameCounter#
EmberGpSecurityFrameCounter EmberGpSinkTableEntry::gpdSecurityFrameCounter
The SFC of the GPD