Public Attribute Documentation#

allocateMemoryForResponses#

bool EmberAfGbzMessageCreatorState::allocateMemoryForResponses

command#

uint8_t* EmberAfGbzMessageCreatorState::command

commandIndex#

uint16_t EmberAfGbzMessageCreatorState::commandIndex

commandLength#

uint16_t EmberAfGbzMessageCreatorState::commandLength

responses#

EmAfGbzUseCaseSpecificComponent* EmberAfGbzMessageCreatorState::responses

lastResponse#

EmAfGbzUseCaseSpecificComponent* EmberAfGbzMessageCreatorState::lastResponse

header#

EmAfGbzPayloadHeader* EmberAfGbzMessageCreatorState::header

nextEncryptedComponentZclSequenceNumber#

uint8_t EmberAfGbzMessageCreatorState::nextEncryptedComponentZclSequenceNumber

nextComponentZclSequenceNumber#

uint8_t EmberAfGbzMessageCreatorState::nextComponentZclSequenceNumber

nextAdditionalHeaderFrameCounter#

uint8_t EmberAfGbzMessageCreatorState::nextAdditionalHeaderFrameCounter

componentsCount#

uint8_t* EmberAfGbzMessageCreatorState::componentsCount

lastExtHeaderControlField#

uint8_t* EmberAfGbzMessageCreatorState::lastExtHeaderControlField

messageCode#

uint16_t EmberAfGbzMessageCreatorState::messageCode

result#

EmberAfGbzMessageCreatorResult EmberAfGbzMessageCreatorState::result