Public Attribute Documentation#

tierSummation#

uint8_t EmberAfSnapshotPayload::tierSummation[SUMMATION_TIERS *6]

tierBlockSummation#

uint8_t EmberAfSnapshotPayload::tierBlockSummation[BLOCK_TIERS *6]

currentSummation#

uint8_t EmberAfSnapshotPayload::currentSummation[6]

billToDate#

uint32_t EmberAfSnapshotPayload::billToDate

billToDateTimeStamp#

uint32_t EmberAfSnapshotPayload::billToDateTimeStamp

projectedBill#

uint32_t EmberAfSnapshotPayload::projectedBill

projectedBillTimeStamp#

uint32_t EmberAfSnapshotPayload::projectedBillTimeStamp

snapshotId#

uint32_t EmberAfSnapshotPayload::snapshotId

snapshotTime#

uint32_t EmberAfSnapshotPayload::snapshotTime

snapshotCause#

uint32_t EmberAfSnapshotPayload::snapshotCause

requestingId#

EmberNodeId EmberAfSnapshotPayload::requestingId

tiersInUse#

uint8_t EmberAfSnapshotPayload::tiersInUse

tiersAndBlocksInUse#

uint8_t EmberAfSnapshotPayload::tiersAndBlocksInUse

srcEndpoint#

uint8_t EmberAfSnapshotPayload::srcEndpoint

dstEndpoint#

uint8_t EmberAfSnapshotPayload::dstEndpoint

billTrailingDigit#

uint8_t EmberAfSnapshotPayload::billTrailingDigit

payloadType#

uint8_t EmberAfSnapshotPayload::payloadType