The information regarding scan results.

Public Attributes#

int8_t
uint8_t
uint8_t
EmberZigbeeNetwork *
uint16_t

Public Attribute Documentation#

status#

sl_status_t EmberAfPluginScanDispatchScanResults::status

The status indicating the success or failure of a scan.

This member is only valid when emberAfPluginScanDispatchScanResultsAreComplete returns true.


Definition at line 59 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

rssi#

int8_t EmberAfPluginScanDispatchScanResults::rssi

The RSSI found during a scan.

This member is only valid when emberAfPluginScanDispatchScanResultsAreComplete returns false.


Definition at line 66 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

channel#

uint8_t EmberAfPluginScanDispatchScanResults::channel

The channel on which the scan is taking place.

This member is only valid when the results are for an energy scan or emberAfPluginScanDispatchScanResultsAreComplete returns true and emberAfPluginScanDispatchScanResultsAreFailure returns false. Note that in active scan results, users can find the channel on which the network was found using the network member of this structure.


Definition at line 76 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

lqi#

uint8_t EmberAfPluginScanDispatchScanResults::lqi

The LQI found during the scan.

This member is only valid when the result are for an active scan.


Definition at line 82 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

network#

EmberZigbeeNetwork* EmberAfPluginScanDispatchScanResults::network

The Zigbee network found in the scan.

This member is only valid when the result are for an active scan.


Definition at line 88 of file app/framework/plugin/scan-dispatch/scan-dispatch.h

mask#

uint16_t EmberAfPluginScanDispatchScanResults::mask

A mask containing information about the scan.


Definition at line 91 of file app/framework/plugin/scan-dispatch/scan-dispatch.h