Concentrator Support#

API and Callbacks for the Concentrator Support Component.

Code that handles periodically broadcasting a many-to-one-route-request (MTORR) so that the device will act as a concentrator (sink) in the network.

  • Note: NCP/SOC source route table size can be now defined as part of the source routing library.

API#

uint32_t

Concentrator source route discovery.

void

Concentrator stop source route discover.

Enumerations#

enum
EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_NONE = NONE
EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL = FULL
EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_MAX = EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL
}

Macros#

#define
LOW_RAM_CONCENTRATOR EMBER_LOW_RAM_CONCENTRATOR
#define
HIGH_RAM_CONCENTRATOR EMBER_HIGH_RAM_CONCENTRATOR
#define
emberAfPluginConcentratorGetRouterBehavior ()
#define
emberAfPluginConcentratorSetRouterBehavior (behavior)

API Documentation#

emberAfPluginConcentratorQueueDiscovery#

uint32_t emberAfPluginConcentratorQueueDiscovery (void )

Concentrator source route discovery.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • uint32_t


emberAfPluginConcentratorStopDiscovery#

void emberAfPluginConcentratorStopDiscovery (void )

Concentrator stop source route discover.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Enumeration Documentation#

EmberAfPluginConcentratorRouterBehavior#

EmberAfPluginConcentratorRouterBehavior
Enumerator
EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_NONE
EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_FULL
EMBER_AF_PLUGIN_CONCENTRATOR_ROUTER_BEHAVIOR_MAX

Typedef Documentation#

EmberAfPluginConcentratorRouterBehavior#

typedef uint8_t EmberAfPluginConcentratorRouterBehavior

Variable Documentation#

emberAfPluginConcentratorUpdateEventControl#

EmberEventControl emberAfPluginConcentratorUpdateEventControl

sli_zigbee_af_concentrator_router_behaviors#

EmberAfPluginConcentratorRouterBehavior sli_zigbee_af_concentrator_router_behaviors[]