Modules#

WWAH Connectivity Manager

WWAH Connectivity Manager#

API and Callbacks for the WWAH Connectivity Manager Component.

Silicon Labs implementation of the Works With All Hubs connectivity functions per the Zigbee WWAH Requirements document. This component should be included by routers and end devices only. This component manages connectivity states to both the hub and, for end devices, to the parent. In the event of connection loss, restoration is performed per the WWAH Connectivity Recovery Procedure as defined in the Zigbee WWAH Requirements specification. The component uses the Trust Center Keepalive component on routers and non-sleepy end devices to determine hub connectivity. On sleepy end devices, it uses the Poll Control Server component to determine hub connectivity. On end devices, this component also uses the End Device Support component to determine parent connectivity.

API#

bool

Get rejoin algorithm enabled state.

void

Enable rejoin algorithm.

void

Disable rejoin algorithm.

void

Enable bad parent recovery.

EmberStatus

Enable periodic router checkins.

EmberStatus
void
emberAfPluginWwahConnectivityManagerSetRejoinParameters(uint16_t fastRejoinTimeoutSeconds, uint16_t durationBetweenRejoinsSeconds, uint16_t fastRejoinFirstBackoffSeconds, uint16_t maxBackoffTimeSeconds, uint16_t maxBackoffIterations)

Set rejoin parameters.

API Documentation#

emberAfPluginWwahConnectivityManagerIsRejoinAlgorithmEnabled#

bool emberAfPluginWwahConnectivityManagerIsRejoinAlgorithmEnabled (void )

Get rejoin algorithm enabled state.

Parameters
N/A

Returns

  • bool true if enabled


Definition at line 54 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerEnableRejoinAlgorithm#

void emberAfPluginWwahConnectivityManagerEnableRejoinAlgorithm (uint8_t endpoint)

Enable rejoin algorithm.

Parameters
N/Aendpoint

Ver.: always


Definition at line 61 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerDisableRejoinAlgorithm#

void emberAfPluginWwahConnectivityManagerDisableRejoinAlgorithm (uint8_t endpoint)

Disable rejoin algorithm.

Parameters
N/Aendpoint

Ver.: always


Definition at line 68 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerIsBadParentRecoveryEnabled#

bool emberAfPluginWwahConnectivityManagerIsBadParentRecoveryEnabled (void )

Get bad parent recovery state.

Parameters
N/A

Returns

  • bool true if enabled


Definition at line 75 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerEnableBadParentRecovery#

void emberAfPluginWwahConnectivityManagerEnableBadParentRecovery (uint16_t badParentRejoinPeriod)

Enable bad parent recovery.

Parameters
N/AbadParentRejoinPeriod

Ver.: always


Definition at line 82 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerDisableBadParentRecovery#

void emberAfPluginWwahConnectivityManagerDisableBadParentRecovery ()

Disable bad parent recovery.


Definition at line 87 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerEnablePeriodicRouterCheckIns#

EmberStatus emberAfPluginWwahConnectivityManagerEnablePeriodicRouterCheckIns (uint16_t checkInInterval)

Enable periodic router checkins.

Parameters
N/AcheckInInterval

Ver.: always

Returns

  • EmberStatus status code


Definition at line 96 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerDisablePeriodicRouterCheckIns#

EmberStatus emberAfPluginWwahConnectivityManagerDisablePeriodicRouterCheckIns (void )

Disable periodic router checkins.

Parameters
N/A

Returns

  • EmberStatus status code


Definition at line 103 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h

emberAfPluginWwahConnectivityManagerSetRejoinParameters#

void emberAfPluginWwahConnectivityManagerSetRejoinParameters (uint16_t fastRejoinTimeoutSeconds, uint16_t durationBetweenRejoinsSeconds, uint16_t fastRejoinFirstBackoffSeconds, uint16_t maxBackoffTimeSeconds, uint16_t maxBackoffIterations)

Set rejoin parameters.

Parameters
N/AfastRejoinTimeoutSeconds

Ver.: always

N/AdurationBetweenRejoinsSeconds

Ver.: always

N/AfastRejoinFirstBackoffSeconds

Ver.: always

N/AmaxBackoffTimeSeconds

Ver.: always

N/AmaxBackoffIterations

Ver.: always


Definition at line 114 of file app/framework/plugin/wwah-connectivity-manager/wwah-connectivity-manager.h