Modules#
MAC Address Filtering#
API and Callbacks for the MAC Address Filtering Component.
This plugin artificially limits what the stack hears by filtering the packets just above the lower MAC. The plugin can be configured on the fly via CLI with the short or long address of devices whose packets will be dropped or allowed. There are two lists, a short address list (2-byte node ID) and a long address list (8-byte IEEE address). Each list may be configured as either an allow list or block list. The default is a block list with no addresses configured (accept all packets normally). A separate option allows or drops packets with no address information (e.g., Beacon Requests). NOTE: The radio will still generate and process MAC ACKs for packets. This plugin cannot be used to effect the behavior of MAC ACKs, which are handled by the RAIL library and radio hardware.
API#
Print configuration command.
Filter out the no address command.
Add the short address command.
Set the short address list type.
Set the long address list type.
Add long address.
Clear the short address list.
Clear the long address list.
Add panID.
Delete a panID entry.
Clear the panID list.
Set the list type for panID list.
MAC address filtering reset.
Clear all lists for MAC address filtering.
Delete an entry from short address list.
Delete an entry from long address list.
Get stats for a short address.
Get MAC address filtering stats. Get the allowed, dropped and total packet counts.
API Documentation#
emberAfPluginMacAddressFilteringPrintConfigCommand#
void emberAfPluginMacAddressFilteringPrintConfigCommand (sl_cli_command_arg_t * arguments)
Print configuration command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringFilterNoAddressCommand#
void emberAfPluginMacAddressFilteringFilterNoAddressCommand (sl_cli_command_arg_t * arguments)
Filter out the no address command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringAddShortAddressCommand#
void emberAfPluginMacAddressFilteringAddShortAddressCommand (sl_cli_command_arg_t * arguments)
Add the short address command.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringSetShortAddressListType#
void emberAfPluginMacAddressFilteringSetShortAddressListType (sl_cli_command_arg_t * arguments)
Set the short address list type.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringSetLongAddressListType#
void emberAfPluginMacAddressFilteringSetLongAddressListType (sl_cli_command_arg_t * arguments)
Set the long address list type.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringAddLongAddressCommand#
void emberAfPluginMacAddressFilteringAddLongAddressCommand (sl_cli_command_arg_t * arguments)
Add long address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringClearShortAddressList#
void emberAfPluginMacAddressFilteringClearShortAddressList (sl_cli_command_arg_t * arguments)
Clear the short address list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringClearLongAddressList#
void emberAfPluginMacAddressFilteringClearLongAddressList (sl_cli_command_arg_t * arguments)
Clear the long address list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringAddPanIdCommand#
void emberAfPluginMacAddressFilteringAddPanIdCommand (sl_cli_command_arg_t * arguments)
Add panID.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringPanIdDeleteEntry#
void emberAfPluginMacAddressFilteringPanIdDeleteEntry (sl_cli_command_arg_t * arguments)
Delete a panID entry.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringClearPanIdList#
void emberAfPluginMacAddressFilteringClearPanIdList (sl_cli_command_arg_t * arguments)
Clear the panID list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringSetPanIdListType#
void emberAfPluginMacAddressFilteringSetPanIdListType (sl_cli_command_arg_t * arguments)
Set the list type for panID list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringReset#
void emberAfPluginMacAddressFilteringReset (sl_cli_command_arg_t * arguments)
MAC address filtering reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringClearAll#
void emberAfPluginMacAddressFilteringClearAll (void )
Clear all lists for MAC address filtering.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A | * arguments Ver.: always |
emberAfPluginMacAddressFilteringShortAddressDeleteEntry#
void emberAfPluginMacAddressFilteringShortAddressDeleteEntry (sl_cli_command_arg_t * arguments)
Delete an entry from short address list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringLongAddressDeleteEntry#
void emberAfPluginMacAddressFilteringLongAddressDeleteEntry (sl_cli_command_arg_t * arguments)
Delete an entry from long address list.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_cli_command_arg_t * | N/A | arguments | * arguments Ver.: always |
emberAfPluginMacAddressFilteringGetStatsForShortAddress#
EmberStatus emberAfPluginMacAddressFilteringGetStatsForShortAddress (uint8_t index, uint32_t * matchCountForIndexPtr)
Get stats for a short address.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | N/A | index | Ver.: always |
| uint32_t * | N/A | matchCountForIndexPtr | Ver.: always |
Returns
EmberStatus status code
emberAfPluginMacAddressFilteringGetStats#
void emberAfPluginMacAddressFilteringGetStats (bool shortMode, uint32_t * allowedPacketCountPtr, uint32_t * droppedPacketCountPtr, uint32_t * totalPacketCountPtr)
Get MAC address filtering stats. Get the allowed, dropped and total packet counts.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bool | N/A | shortMode | Ver.: always |
| uint32_t * | N/A | allowedPacketCountPtr | Ver.: always |
| uint32_t * | N/A | droppedPacketCountPtr | Ver.: always |
| uint32_t * | N/A | totalPacketCountPtr | Ver.: always |