Find and Bind Target#

API and Callbacks for the Find and Bind Target Component.

This component provides the functionality for a target device to start identifying on user-defined endpoints. The target device can then act as a target for a finding and binding initiator.

API#

Start target finding and binding operations.

Macros#

#define
EMBER_AF_PLUGIN_FIND_AND_BIND_TARGET_PLUGIN_NAME "Find and Bind Target"

API Documentation#

emberAfPluginFindAndBindTargetStart#

EmberAfStatus emberAfPluginFindAndBindTargetStart (uint8_t endpoint)

Start target finding and binding operations.

Parameters
N/Aendpoint

The endpoint on which to begin target operations.

A call to this function will commence the target finding and binding operations. Specifically, the target will attempt to start identifying on the endpoint that is passed as a parameter.

Returns

  • An EmberAfStatus value describing the success of the commencement of the target operations.


Definition at line 61 of file app/framework/plugin/find-and-bind-target/find-and-bind-target.h