Prepayment Client#
API and Callbacks for the Prepayment Cluster Client Component.
This component implements the client-side functionality of the Smart Energy 1.2 Prepayment cluster.
Modules#
API#
void
emberAfPluginPrepaymentClientChangePaymentMode(EmberNodeId nodeId, uint8_t srcEndpoint, uint8_t dstEndpoint, uint32_t providerId, uint32_t issuerEventId, uint32_t implementationDateTime, uint16_t proposedPaymentControlConfiguration, uint32_t cutOffValue)
change prepayment client payment mode
API Documentation#
emberAfPluginPrepaymentClientChangePaymentMode#
void emberAfPluginPrepaymentClientChangePaymentMode (EmberNodeId nodeId, uint8_t srcEndpoint, uint8_t dstEndpoint, uint32_t providerId, uint32_t issuerEventId, uint32_t implementationDateTime, uint16_t proposedPaymentControlConfiguration, uint32_t cutOffValue)
change prepayment client payment mode
Parameters
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberNodeId | N/A | nodeId | Ver.: always |
| uint8_t | N/A | srcEndpoint | Ver.: always |
| uint8_t | N/A | dstEndpoint | Ver.: always |
| uint32_t | N/A | providerId | Ver.: always |
| uint32_t | N/A | issuerEventId | Ver.: always |
| uint32_t | N/A | implementationDateTime | Ver.: always |
| uint16_t | N/A | proposedPaymentControlConfiguration | Ver.: always |
| uint32_t | N/A | cutOffValue | Ver.: always |