Scan Dispatch#
API and Callbacks for the scan-dispatch Component.
This component allows existence of multiple consumers of the stack 802.15.4 scan results.
This plugin allows for multiple consumers of stack 802.15.4 scan callbacks.
Modules#
EmberAfPluginScanDispatchScanResults
EmberAfPluginScanDispatchScanData
API#
Get the scan type.
Get whether the originally requested scan has completed.
Result in a failure.
Schedule a scan.
Remove all consumers in the queue.
Typedefs#
Handle scan results.
Macros#
The size of the dispatch queue.
API Documentation#
emberAfPluginScanDispatchScanResultsGetScanType#
EmberNetworkScanType emberAfPluginScanDispatchScanResultsGetScanType (EmberAfPluginScanDispatchScanResults * results)
Get the scan type.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberAfPluginScanDispatchScanResults * | N/A | results | The EmberAfPluginScanDispatchScanResults for which the scan type will be found. |
Gets the scan type from an EmberAfPluginScanDispatchScanResults. This value will either be ::EMBER_ENERGY_SCAN, ::EMBER_ACTIVE_SCAN or ::EMBER_ACTIVE_SCAN_ROUTER
Returns
The ::EmberNetworkScanType of the scan results.
emberAfPluginScanDispatchScanResultsAreComplete#
bool emberAfPluginScanDispatchScanResultsAreComplete (EmberAfPluginScanDispatchScanResults * results)
Get whether the originally requested scan has completed.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberAfPluginScanDispatchScanResults * | N/A | results | The EmberAfPluginScanDispatchScanResults that belong to a potentially complete scan. |
This can happen either when the dispatcher asks the stack for a scan (see ::emberStartScan) or after all of the scan results have been delivered to the consumer (see emberAfScanCompleteCallback).
Returns
Indicates whether or not the scan for the scan results is complete.
emberAfPluginScanDispatchScanResultsAreFailure#
bool emberAfPluginScanDispatchScanResultsAreFailure (EmberAfPluginScanDispatchScanResults * results)
Result in a failure.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberAfPluginScanDispatchScanResults * | N/A | results | The EmberAfPluginScanDispatchScanResults for which the call to ::emberStartScan may have failed. |
Gets whether or not the scan results are from a failed call to ::emberStartScan.
Returns
Indicates whether or not the call to ::emberStartScan failed for these results.
emberAfPluginScanDispatchScheduleScan#
EmberStatus emberAfPluginScanDispatchScheduleScan (EmberAfPluginScanDispatchScanData * data)
Schedule a scan.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| EmberAfPluginScanDispatchScanData * | N/A | data | An EmberAfPluginScanDispatchScanData that holds the scanType, channelMask, duration, and EmberAfPluginScanDispatchScanResultsHandler for the scan. |
This API schedules an 802.15.4 scan. The results will be delivered to the consumer via a handler in the passed EmberAfPluginScanDispatchScanData.
Returns
An ::EmberStatus value describing the result of the scheduling of a scan.
emberAfPluginScanDispatchClear#
void emberAfPluginScanDispatchClear (void )
Remove all consumers in the queue.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
A call to this function will remove all consumers in the queue for scan results. It will also cancel any 802.15.4 scan that the stack is currently performing.