Application information. During the commissioning of GPD that supports generic switch, multi sensor extension and compact report attribute the application information is exchanged as part of the GPD commissioning command 0xE0 and 0xE4. This structure holds the information for the commissioned GPD.
Public Attributes#
uint8_t
uint8_t
uint16_t
uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t
uint16_t
uint16_t
Public Attribute Documentation#
numberOfGpdCommands#
uint8_t EmberGpApplicationInfo::numberOfGpdCommands
Number of GPD commands supported by the GPD
gpdCommands#
uint8_t EmberGpApplicationInfo::gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1]
Supported GPD Commands
numberOfPairedEndpoints#
uint8_t EmberGpApplicationInfo::numberOfPairedEndpoints
Number of paired endpoints for the GPD
pairedEndpoints#
uint8_t EmberGpApplicationInfo::pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1]
Paired endpoints
numberOfGpdClientCluster#
uint8_t EmberGpApplicationInfo::numberOfGpdClientCluster
Number of operational client clusters present on the GPD, maximum is 15.
numberOfGpdServerCluster#
uint8_t EmberGpApplicationInfo::numberOfGpdServerCluster
Number of operational server clusters present on the GPD, maximum is 15.
serverClusters#
uint16_t EmberGpApplicationInfo::serverClusters[15]
Operational server clusters present on the GPD
clientClusters#
uint16_t EmberGpApplicationInfo::clientClusters[15]
Operational client clusters present on the GPD