Generic Switch Information. Generic switch feature uses this as descriptor to interpret the incoming switch command from the GPD. This information is set up at the sink during the commissioning.

Public Attributes#

uint8_t

Public Attribute Documentation#

switchInfoLength#

uint8_t EmberGpSwitchInformation::switchInfoLength

Switch Information Length


nbOfContacts#

uint8_t EmberGpSwitchInformation::nbOfContacts

Number of contacts in the switch


switchType#

uint8_t EmberGpSwitchInformation::switchType

Switch type


currentContact#

uint8_t EmberGpSwitchInformation::currentContact

Current contact


savedContact#

uint8_t EmberGpSwitchInformation::savedContact

Saved contacts