Describe the time in a human understandable format (as opposed to 32-bit UTC).

Public Attributes#

uint16_t
uint8_t
uint8_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

year#

uint16_t EmberAfTimeStruct::year

Definition at line 1589 of file app/framework/include/af-types.h

month#

uint8_t EmberAfTimeStruct::month

Definition at line 1590 of file app/framework/include/af-types.h

day#

uint8_t EmberAfTimeStruct::day

Definition at line 1591 of file app/framework/include/af-types.h

hours#

uint8_t EmberAfTimeStruct::hours

Definition at line 1592 of file app/framework/include/af-types.h

minutes#

uint8_t EmberAfTimeStruct::minutes

Definition at line 1593 of file app/framework/include/af-types.h

seconds#

uint8_t EmberAfTimeStruct::seconds

Definition at line 1594 of file app/framework/include/af-types.h