Use for all trust center backup data.

The 'keyList' pointer must point to an array and 'maxKeyListLength' must be populated with the maximum number of entries the array can hold.

Functions that modify this data structure will populate 'keyListLength' indicating how many keys were actually written into 'keyList'.

Public Attribute Documentation#

extendedPanId#

EmberEUI64 EmberAfTrustCenterBackupData::extendedPanId

Definition at line 1545 of file app/framework/include/af-types.h

keyListLength#

uint8_t EmberAfTrustCenterBackupData::keyListLength

Definition at line 1546 of file app/framework/include/af-types.h

maxKeyListLength#

uint8_t EmberAfTrustCenterBackupData::maxKeyListLength

Definition at line 1547 of file app/framework/include/af-types.h

keyList#

EmberAfLinkKeyBackupData* EmberAfTrustCenterBackupData::keyList

Definition at line 1548 of file app/framework/include/af-types.h