Represent Endpoint Information Records used by ZLL Commissioning.

Public Attributes#

EmberNodeId
uint8_t
uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

networkAddress#

EmberNodeId EmberAfPluginZllCommissioningEndpointInformationRecord::networkAddress

Definition at line 1188 of file app/framework/include/af-types.h

endpointId#

uint8_t EmberAfPluginZllCommissioningEndpointInformationRecord::endpointId

Definition at line 1189 of file app/framework/include/af-types.h

profileId#

uint16_t EmberAfPluginZllCommissioningEndpointInformationRecord::profileId

Definition at line 1190 of file app/framework/include/af-types.h

deviceId#

uint16_t EmberAfPluginZllCommissioningEndpointInformationRecord::deviceId

Definition at line 1191 of file app/framework/include/af-types.h

version#

uint8_t EmberAfPluginZllCommissioningEndpointInformationRecord::version

Definition at line 1192 of file app/framework/include/af-types.h