Structure for ZCL command "QuerySpecificFileRequest" from "Over the Air Bootloading".
Public Attribute Documentation#
requestNodeAddress#
uint8_t* __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::requestNodeAddress
manufacturerId#
uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::manufacturerId
imageType#
uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::imageType
fileVersion#
uint32_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::fileVersion
currentZigbeeStackVersion#
uint16_t __zcl_over_the_air_bootloading_cluster_query_specific_file_request_command::currentZigbeeStackVersion