Address for sending and receiving a CGp message.

Public Attributes#

sl_802154_short_addr_t
sl_802154_long_addr_t
union sl_zigbee_c_gp_address_t::@8
sl_802154_pan_id_t

Public Attribute Documentation#

shortId#

sl_802154_short_addr_t sl_zigbee_c_gp_address_t::shortId

The 16-bit short address is used when the mode is SL_ZIGBEE_CGP_ADDRESS_MODE_SHORT.


extendedId#

sl_802154_long_addr_t sl_zigbee_c_gp_address_t::extendedId

The 64-bit extended address is used when the mode is SL_ZIGBEE_CGP_ADDRESS_MODE_EXTENDED.


address#

union sl_zigbee_c_gp_address_t::@8 sl_zigbee_c_gp_address_t::address

The address.


panId#

sl_802154_pan_id_t sl_zigbee_c_gp_address_t::panId

The PAN identifier is used when the mode is not SL_ZIGBEE_CGP_ADDRESS_MODE_NONE.


mode#

sl_zigbee_c_gp_address_mode_t sl_zigbee_c_gp_address_t::mode

The addressing mode.