Switch Information.
Public Attribute Documentation#
currentStatus#
uint8_t sl_zigbee_gp_generic_switch_data_t::currentStatus
provides button information of the Generic switch for the current contacts status
contactBitmask#
uint8_t sl_zigbee_gp_generic_switch_data_t::contactBitmask
Provides the bitmask to evaluate the received contact. As a result, the bitmask only depends on the number of contacts of the current GPD.