The internal representation of a sink table entry.
Public Attribute Documentation#
status#
sl_zigbee_gp_sink_table_entry_status_t sl_zigbee_gp_sink_table_entry_t::status
Internal status. Defines if the entry is unused or used as a sink table entry
Definition at line
431
of file stack/include/gp-types.h
options#
uint16_t sl_zigbee_gp_sink_table_entry_t::options
The tunneling options (this contains both options and extendedOptions from the spec)
Definition at line
435
of file stack/include/gp-types.h
gpd#
sl_zigbee_gp_address_t sl_zigbee_gp_sink_table_entry_t::gpd
The addressing info of the GPD
Definition at line
439
of file stack/include/gp-types.h
deviceId#
uint8_t sl_zigbee_gp_sink_table_entry_t::deviceId
The device ID for the GPD
Definition at line
443
of file stack/include/gp-types.h
sinkList#
sl_zigbee_gp_sink_list_entry_t sl_zigbee_gp_sink_table_entry_t::sinkList[GP_SINK_LIST_ENTRIES]
The list of sinks; hardcoded to 2, which is the spec minimum
Definition at line
447
of file stack/include/gp-types.h
assignedAlias#
sl_802154_short_addr_t sl_zigbee_gp_sink_table_entry_t::assignedAlias
The assigned alias for the GPD
Definition at line
451
of file stack/include/gp-types.h
groupcastRadius#
uint8_t sl_zigbee_gp_sink_table_entry_t::groupcastRadius
The groupcast radius
Definition at line
455
of file stack/include/gp-types.h
securityOptions#
uint8_t sl_zigbee_gp_sink_table_entry_t::securityOptions
The security options field
Definition at line
459
of file stack/include/gp-types.h
gpdSecurityFrameCounter#
sl_zigbee_gp_security_frame_counter_t sl_zigbee_gp_sink_table_entry_t::gpdSecurityFrameCounter
The SFC of the GPD
Definition at line
463
of file stack/include/gp-types.h
gpdKey#
sl_zigbee_key_data_t sl_zigbee_gp_sink_table_entry_t::gpdKey
The GPD key associated with this entry.
Definition at line
467
of file stack/include/gp-types.h