You are viewing documentation for version:
Data point descriptor. Compact attribute, Multi sensor or Generic switch feature uses this as descriptor to interpret the incoming data from the GPD. This descriptor is set up at the sink during the commissioning. 
Public Attribute Documentation#
nbAttrRecord#
uint8_t sl_zigbee_gp_data_point_descriptor_t::nbAttrRecord
Number of attribute records 
clientServer#
uint8_t sl_zigbee_gp_data_point_descriptor_t::clientServer
Client or Server flag 
ManIdPresent#
uint8_t sl_zigbee_gp_data_point_descriptor_t::ManIdPresent
Manufacture ID present 
datapointOptions#
uint8_t sl_zigbee_gp_data_point_descriptor_t::datapointOptions
Data point options 
clusterID#
uint16_t sl_zigbee_gp_data_point_descriptor_t::clusterID
Cluster ID 
manufacturerID#
uint16_t sl_zigbee_gp_data_point_descriptor_t::manufacturerID
Manufacture ID 
attrRecord#
sl_zigbee_gp_attribute_record_t sl_zigbee_gp_data_point_descriptor_t::attrRecord
Attribute Record