Application information. During the commissioning of GPD that supports generic switch, multi sensor extension and compact report attribute the application information is exchanged as part of the GPD commissioning command 0xE0 and 0xE4. This structure holds the information for the commissioned GPD.

Public Attribute Documentation#

deviceId#

uint8_t sl_zigbee_gp_application_info_t::deviceId

Device ID of the GPD


Definition at line 588 of file stack/include/gp-types.h

applInfoBitmap#

uint8_t sl_zigbee_gp_application_info_t::applInfoBitmap

Application Information bitmap


Definition at line 590 of file stack/include/gp-types.h

manufacturerId#

uint16_t sl_zigbee_gp_application_info_t::manufacturerId

Manufacturer ID of the GPD


Definition at line 592 of file stack/include/gp-types.h

modelId#

uint16_t sl_zigbee_gp_application_info_t::modelId

Model ID of the GPD


Definition at line 594 of file stack/include/gp-types.h

numberOfGpdCommands#

uint8_t sl_zigbee_gp_application_info_t::numberOfGpdCommands

Number of GPD commands supported by the GPD


Definition at line 596 of file stack/include/gp-types.h

gpdCommands#

uint8_t sl_zigbee_gp_application_info_t::gpdCommands[GP_COMMISSIONING_MAX_BYTES - 1]

Supported GPD Commands


Definition at line 598 of file stack/include/gp-types.h

numberOfPairedEndpoints#

uint8_t sl_zigbee_gp_application_info_t::numberOfPairedEndpoints

Number of paired endpoints for the GPD


Definition at line 600 of file stack/include/gp-types.h

pairedEndpoints#

uint8_t sl_zigbee_gp_application_info_t::pairedEndpoints[GP_COMMISSIONING_MAX_BYTES - 1]

Paired endpoints


Definition at line 602 of file stack/include/gp-types.h

numberOfGpdClientCluster#

uint8_t sl_zigbee_gp_application_info_t::numberOfGpdClientCluster

Number of operational client clusters present on the GPD, maximum is 15.


Definition at line 604 of file stack/include/gp-types.h

numberOfGpdServerCluster#

uint8_t sl_zigbee_gp_application_info_t::numberOfGpdServerCluster

Number of operational server clusters present on the GPD, maximum is 15.


Definition at line 606 of file stack/include/gp-types.h

serverClusters#

uint16_t sl_zigbee_gp_application_info_t::serverClusters[15]

Operational server clusters present on the GPD


Definition at line 608 of file stack/include/gp-types.h

clientClusters#

uint16_t sl_zigbee_gp_application_info_t::clientClusters[15]

Operational client clusters present on the GPD


Definition at line 610 of file stack/include/gp-types.h